This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP41009: 电路设计

Part Number: PMP41009
Other Parts Discussed in Thread: UCC28740,

Hello, I want to design a wide-range input flyback switching power supply with 120-1350VDC input, 24V output, and 40W output power, referring to the circuit in PMP41009. I would like you to recommend a flyback control chip similar to the UCC28740 chip, with a maximum operating frequency of up to 130KHz. Is there a suitable one?
  • 已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • Hello, I have another question. The chip I selected for the flyback circuit I designed has a built-in high-voltage startup circuit, so there is no need for an external high-voltage startup circuit to provide the initial voltage. The MOSFET I use is a SiC MOSFET, so I added a UCC5350M driver chip to the drive circuit. The chip pins VCC1 and VCC2 are connected to the auxiliary winding. Since the auxiliary winding only starts up after the circuit works normally, I am worried that the driver chip may not function in time, causing the circuit to fail to work properly. Will this situation occur?

  • Hello, may I ask what the suitable maximum duty cycle is for the UCC228740 chip in my design?

  • Hi, Why do you want to use maximum operating frequency 130KHz? I don't recommend so high frequency with the high input voltage 1350V. 

     We need to short the ground 1, 2, 3.