This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP41009: 电路设计

Part Number: PMP41009
Other Parts Discussed in Thread: UCC28740,

Hello, I want to design a wide-range input flyback switching power supply with 120-1350VDC input, 24V output, and 40W output power, referring to the circuit in PMP41009. I would like you to recommend a flyback control chip similar to the UCC28740 chip, with a maximum operating frequency of up to 130KHz. Is there a suitable one?