This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请介绍一下输出电压和电流可以设置的芯片



目标应用是给电池充电,但是充电的各个参数都是可以随时通过软件修改的,需要具有恒压和恒流模式。

要求比较特殊,因为需要很高的精度,需要1%以内最好0.5%精度的电压电流输出。

输出电压和电流没有限制,因为产品的范围比较宽泛,电压电流的要求也是比较多,主要是集中在2-5V,0-12V,0-50V,电流几个安培到几百安培。

谢谢各位!