This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: 技术咨询

Part Number: BQ25756

你好,

      在使用BQ25756时有如下疑惑,请帮忙解答一下,谢谢!

 

1、输入电流采用5mΩ电阻,调节范围400mA~20A,步长为50mA。

问题1:输入电阻最大采样电阻是否可以超过10mΩ?

如果可以超过10mΩ的话,输入电流采样电阻用50mΩ,是不是调节步长就可以变成40mA~2A?调节步长变成5mA?其次40mA以下的电流是否可以继续以5mA的步长继续调节到0A?

如果不可以超过10mΩ,输入电流采样电阻采用10mΩ后,采样范围会变成200mA~10000mA?,调节步长变成25mA?

                          

问题2:充电电流采样可以调节电流采样电阻么?如果可以的话,充电电流采样电阻从5mΩ改成50mΩ后,调节步长是否会变成5mA?

调节范围是否会变成40mA~2000mA?其次40mA以下的电流是否可以继续调节?

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 您好

    问题1:输入电阻最大采样电阻是否可以超过10mΩ?

    是的,阻力可以增加,但不能减少。这有什么特别的原因吗?较大的电阻会降低这里的效率,使用ILIM_HIZ引脚,您仍然可以将输入电流限制在小于2A的值。

    问题2:充电电流采样可以调节电流采样电阻么?如果可以的话,充电电流采样电阻从5mΩ改成50mΩ后,调节步长是否会变成5mA?

    我们不建议更改电池感应电阻值,但我认为增加电阻不会造成任何问题,只会降低效率。低于40mA的电流将无法调整。