This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

氢燃料和锂电池混合动力输出电路



项目背景:无人机锂电池和氢燃料电池混合动力系统
系统动力来源为氢燃料电池和锂电池,其中氢燃料电池输入电压50-80V,燃料电池端输入功率15kW;锂电池为18S,10AH电池,持续放电电流150A,脉冲电流350A,<3s;
无人机系统工作电压60-80V,峰值功率25kW。
项目需求:需要设计一个电源系统,氢燃料电池作为输入端,输出电压70V,输出电流200A,总功率为14kW的DCDC,请问TI是否有对应的方案。
项目进程:目前已经采用4开关buck-boost架构设计了一款,最大功率5.7kW,还是无法满足最大功率;多板并联还需要设计均流,TI是否有其他方案,单板实现至少14kW的功率转换。
氢燃料电池特性是在低压输出大功率,因此实际DCDC工作在升压区间较多