This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25751: BUCK-BOOST 的电感选型

Part Number: BQ25751


Dear

我正在用BQ25751设计一个30V电源输入给24V/4Ah 铅酸电池充电,最大充电电流是1A.

我看规格书中推荐的电感值范围是2.2uF~15uF, DRC是1.75~60mohm, 请问这个值是必须遵循的吗?

还是可以按照实际buck电路进行电感选型?

请帮忙解答一下,谢谢!