This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24195 SW与PGND短路是不是芯片烧坏了

Other Parts Discussed in Thread: BQ24195

最近在使用BQ24195做电源管理,接上18650电池后,芯片发烫,SW端口与PGND短路,因为SW与SYS通过电感相连,所以SYS也是与地短接,是不是芯片烧坏了?或者是能给出什么原因导致的吗?需要电路的话,稍后我把电路贴上来。

  • 当使用其它电源供电时,PMID接口外接其它5V电源会不会对芯片有影响?

  •    没人回复吗?这论坛就这么少的人?官方也没人来解答?

  • 你好,掉电时测量sw脚对gnd的阻抗,如果此时还是短路,说明内部的Q3管损坏了。

    PMID口是一个输出口,不是一个输入口,它是用来输出升压模式的5v或者adapter的电压,不接其他的5V.

    详细的情况,请把你实际使用的电路图发上来进一步的分析,谢谢!

  • 谢谢您的回复,我测了一下SW和地的阻抗,为2.8欧姆,下面是电路图和外接负载的电路图。我用MOS管接负载,NOS管导通时PMID电压降到3V,电感有声响,应该不是电路带不动负载,因为当PMID维持5.13V时,直接接负载没有这现象,只是使用MOS管导通后才有这现象,第二张为MOS管开关电路,麻烦您帮忙看一下有什么问题。

  • 如果你设计用key sw的信号控制PMID向VCC5供电,那么AO3401的S级应该接PMID,D级接VCC5。这样体二极管才不会将PMID一直导通到VCC5.

    是在PMID口测量还是VCC5测量到跌落到3V的现象?

    用示波器观察PMID从boost模式开启到后面跌落到3V的过程,PMID的波形在这个过程中变化的情况如何?

    是否有观察到震荡的现象?

    以上谢谢!

  • 感谢您的回答,我是把AO3401反过来S接PMID用的,原理图画错了,然后,我是在PMID口测得的3V。这种现象是在PMID通过AO3401接负载的情况下,当我由bq24195充电状态下大概PMID电压3.5V左右,直接启动boost模式,然后导通AO3401,PMID电压变为5.13V时,电压会先升到5.13V,然后降到3V左右,应该是电感发出的滴滴滴响声。

    用示波器观察电感两端波形,正常不接负载boost模式下,是1.4382MHz,接上负载降到3V时波形很乱,大概是50Hz。

    然后当PMID保持5V电压打开AO3401接负载时,PMID电压不会降到3V,只是0.05V以内变化。

    请问是什么原因导致的充电模式下启动boost 模式会导致PMID电压降低?还有就是我有一块板子当工作在boost模式时,PMID电压为5.13V,时不时的发出滴滴滴声音,和其它板子电路一样,但是其它板子没这样问题。

  • 怎么又没人回复了?

  • SW短地,相当于把开关管直接短路,自然容易损坏芯片