Other Parts Discussed in Thread: BQ24195
最近在使用BQ24195做电源管理,接上18650电池后,芯片发烫,SW端口与PGND短路,因为SW与SYS通过电感相连,所以SYS也是与地短接,是不是芯片烧坏了?或者是能给出什么原因导致的吗?需要电路的话,稍后我把电路贴上来。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: BQ24195
最近在使用BQ24195做电源管理,接上18650电池后,芯片发烫,SW端口与PGND短路,因为SW与SYS通过电感相连,所以SYS也是与地短接,是不是芯片烧坏了?或者是能给出什么原因导致的吗?需要电路的话,稍后我把电路贴上来。
你好,掉电时测量sw脚对gnd的阻抗,如果此时还是短路,说明内部的Q3管损坏了。
PMID口是一个输出口,不是一个输入口,它是用来输出升压模式的5v或者adapter的电压,不接其他的5V.
详细的情况,请把你实际使用的电路图发上来进一步的分析,谢谢!
如果你设计用key sw的信号控制PMID向VCC5供电,那么AO3401的S级应该接PMID,D级接VCC5。这样体二极管才不会将PMID一直导通到VCC5.
是在PMID口测量还是VCC5测量到跌落到3V的现象?
用示波器观察PMID从boost模式开启到后面跌落到3V的过程,PMID的波形在这个过程中变化的情况如何?
是否有观察到震荡的现象?
以上谢谢!
感谢您的回答,我是把AO3401反过来S接PMID用的,原理图画错了,然后,我是在PMID口测得的3V。这种现象是在PMID通过AO3401接负载的情况下,当我由bq24195充电状态下大概PMID电压3.5V左右,直接启动boost模式,然后导通AO3401,PMID电压变为5.13V时,电压会先升到5.13V,然后降到3V左右,应该是电感发出的滴滴滴响声。
用示波器观察电感两端波形,正常不接负载boost模式下,是1.4382MHz,接上负载降到3V时波形很乱,大概是50Hz。
然后当PMID保持5V电压打开AO3401接负载时,PMID电压不会降到3V,只是0.05V以内变化。
请问是什么原因导致的充电模式下启动boost 模式会导致PMID电压降低?还有就是我有一块板子当工作在boost模式时,PMID电压为5.13V,时不时的发出滴滴滴声音,和其它板子电路一样,但是其它板子没这样问题。