当bq24195通过PMOS管接负载,MOS管导通后5.13V就被拉低到3V,而且伴随着电感滴滴滴的响声,这是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
当bq24195通过PMOS管接负载,MOS管导通后5.13V就被拉低到3V,而且伴随着电感滴滴滴的响声,这是什么原因?
急急急!!!!对于带负载电感发出滴滴滴叫声的问题暂时解决了,换个电感值大点的电感就好了,带负载能力比原来强了,我换的是33uH的电感,PMID端接的是22+22+10+10+10=74uF的电容。但是还有个问题是,在启动boost模式后,我接负载时,有的板子还是会降到3V,其它板子有正常的,也有有这问题的。负载功率不大,超不过0.3w,我想请问这是带负载能力低还是电路问题?需不需要换个更大阻止的电感或者换更大容值的电容?
Hi
BQ24195的推荐电感值是2.2uH, 建议把电感量选小一点,且饱和电流至少要5A以上才能带负载,谢谢!
Hisen