This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24195接通负载后电压被拉低

Other Parts Discussed in Thread: BQ24195

当bq24195通过PMOS管接负载,MOS管导通后5.13V就被拉低到3V,而且伴随着电感滴滴滴的响声,这是什么原因?

  • 亲;你是啥位置接5.1V负载?这个系统里;只要SYS通过MOS接电池,只要电池超4.2V,系统就会保护;延时后再开启。这样就发生了你说的现象。所以;正常逻辑是外部有电;MOS关闭由适配器供电,反之用电池供电。

  • 谢谢回复,我是PMID口接的负载,没有使用适配器,我使用的是电池,SYS引脚是悬空的。待机时bq24195设置为充电状态,PMID电压3.5V左右,直接启动boost模式,接通负载,PMID电压会先升到5.13V,然后降到3V左右,电感发出的滴滴滴响声。

  • 急急急!!!!对于带负载电感发出滴滴滴叫声的问题暂时解决了,换个电感值大点的电感就好了,带负载能力比原来强了,我换的是33uH的电感,PMID端接的是22+22+10+10+10=74uF的电容。但是还有个问题是,在启动boost模式后,我接负载时,有的板子还是会降到3V,其它板子有正常的,也有有这问题的。负载功率不大,超不过0.3w,我想请问这是带负载能力低还是电路问题?需不需要换个更大阻止的电感或者换更大容值的电容?

  • 很大可能是PCB Layout的问题,建议严格按照我们Datasheet中Fig 43的建议来进行PCB布局

  • Hi 

    BQ24195的推荐电感值是2.2uH, 建议把电感量选小一点,且饱和电流至少要5A以上才能带负载,谢谢!

    Hisen