This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28C56H-Q1: 参考规格书应用设计,芯片VDD 管脚周期性处于欠压状态,VREF不能正常工作,输出电压不对

Part Number: UCC28C56H-Q1


参考数据手册9.2节应用电路设计,电路无法正常工作。烦请给出排查方向。

高压电压为60V,调整至300V还是会存在一下问题。增大VDD并联电容容值,波动周期会改变,但还是存在欠压情况。调整FB反馈电压阻值,及调整VDD稳态电压值,并没有得到改善,还是会出现电源欠压情况。

看波形类似于二次侧输出短路或过流,但测量输出,未发现短路现象。增加二次侧负载,也还是会存在相同问题。

测试VDD管脚波形,周期性波动

测试Vref管脚波形

测试FB管脚波形

测试二次侧输出波形(忽略后面振荡波形)