This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: 2KW充电器

Part Number: UCC28950
Other Parts Discussed in Thread: UCC28951, , UCC28250

1、如上图,a1选4的话,典型占空比0.67比最大占空比0.66还大,是不是只能选3?

2、如上,谐振电感感值为负数?可以不用?

3、谐振电感的计算感值应该为主电感的漏感+谐振电感的值吗?

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 你好,

    对于2 kW的充电器,UCC28950或具有零电压开关的UCC28951将是比硬开关UCC28250更好的选择。零电压开关意味着没有开关损耗,设计效率更高。
    您可以在以下链接中找到2 kW电池充电器中的UCC28951示例。www.ti.com/.../PMP8740
    excel电子表格中的最大占空比不是UCC28950/1占空比的限制。这些器件可以很容易地实现90%的占空比。这是在最小输入电压下计算a1的推荐目标。Dtyp是从规格表中选择的具有典型输入电压的a1的占空比。
    如果Ls为负,这意味着从100%到50%的负载不需要Ls来实现ZVS。
    谐振电感是Ls和Lpm的组合。