Other Parts Discussed in Thread: BQ24650
我现在在做使用BQ24650芯片的太阳能充电器,目前发现接上电池输出电流很小,用太阳能模拟器供电,输出26V,24650设置mppt最大点为18V,Pack Thermistor接10K电阻到地,Q12没接,接上3cell锂电池也就是大概10V然后再上电,VREF为3.3V,REGN电压6V,STAT1接上的LED亮,STAT2不亮,SRP和SEN之间电压为0.17mV,也就是说没有电流输出。
用的mos管是irf4310,电感10mH,电流采样电阻20毫欧,也就是说设置恒流充电电流2A
很奇怪的是,我用可调电源并联电阻模拟电池,当可调电源电压上升到12.6V(设置的电池饱和电压),STAT1灭,STAT2亮,证明电池检测是好的。
现在的问题就是为什么没有输出,理论说会有30min的预充电,但是电流也会有200MA才对
请教各位,我该怎么办