This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ24650输出问题

Other Parts Discussed in Thread: BQ24650

我现在在做使用BQ24650芯片的太阳能充电器,目前发现接上电池输出电流很小,用太阳能模拟器供电,输出26V,24650设置mppt最大点为18V,Pack Thermistor接10K电阻到地,Q12没接,接上3cell锂电池也就是大概10V然后再上电,VREF为3.3V,REGN电压6V,STAT1接上的LED亮,STAT2不亮,SRP和SEN之间电压为0.17mV,也就是说没有电流输出。

用的mos管是irf4310,电感10mH,电流采样电阻20毫欧,也就是说设置恒流充电电流2A

很奇怪的是,我用可调电源并联电阻模拟电池,当可调电源电压上升到12.6V(设置的电池饱和电压),STAT1灭,STAT2亮,证明电池检测是好的。

现在的问题就是为什么没有输出,理论说会有30min的预充电,但是电流也会有200MA才对

请教各位,我该怎么办