Part Number: BQ4050
我们遇到一个问题,当按键与地之间接1K电阻时,分压拉不低。想知道DISP是如何上拉的,手册上写disp与PBI之间是8kΩ,具体情况是连接到哪里,我们测试了DISP电压值约为4.5V,此电压值是参考哪些参数而来,内部上拉详情是如何?我们是否可以直接改用0Ω电阻,有无具体约束条件?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ4050
我们遇到一个问题,当按键与地之间接1K电阻时,分压拉不低。想知道DISP是如何上拉的,手册上写disp与PBI之间是8kΩ,具体情况是连接到哪里,我们测试了DISP电压值约为4.5V,此电压值是参考哪些参数而来,内部上拉详情是如何?我们是否可以直接改用0Ω电阻,有无具体约束条件?

您好,
可以使用0欧电阻。
请参考bq4050 CEDV Gas Gauge and Protection Solution for 1-Series to 4-Series Cell Li-Ion Battery Packs datasheet (Rev. B) 中“Figure 21. Application Schematic”的电路,按键另一端直接接地。
您好,
DISP脚的内部结构没有更多资源参考。
数据手册第6页提供了“High Voltage I/O”的PRES的内部结构,您可以参考一下。
同样,PBI的内部结构在第5页。
您好,
8K是最小值,不是典型值。
PRES和DISP同作为High Voltage I/O,上拉应该是类似的。
请等待您另一个帖子英文产品线专家的回复。