Other Parts Discussed in Thread: OPA2735, , LM2776
你好,我想请教一下 使用LM27762芯片给OPA2735供电,整个原理图有不妥的地方嘛?另外使用LM27762 供电5V,正输出的电压为4.8V,负端输出只有-2v左右,而且供电1分钟不到芯片很烫,可以帮我看一下是哪里的问题嘛?
电路图中的LM27762部分看起来不错,但是C15应该是4.7uF。布局可以优化,使C14、C13、C16、R13和R15的GND连接更短地连接到LM2776。这将优化寄生电感和潜在的移位。
按照绿色所示移动组件(大小不准确,但我想展示端子应该放置的位置。
我还建议检查负VOUT的过载情况。如果可能,请移除OPA2735,以查看低输出电压是否是由于附加电路造成的。
数据手册8.2.2.5.2 Input Capacitor
In typical applications, a 4.7-µF low-ESR ceramic capacitor is recommended on the input. When operating near the maximum load of 250 mA, after taking into the DC bias derating, a minimum recommended input capacitance is 2 µF or larger. Different input capacitance values can be used to reduce ripple, shrink the solution size, and/or cut the cost of the solution.