Other Parts Discussed in Thread: LM5145, LM5146
想使用LM5116设计可调输出电源,输入48V,输出最低9V,最高16V(功率100W)。
使用WEBENCH在线仿真发现9V和16V输出时,调整固定电感值为6.8uH,然后发现COMP引脚及RAMP引脚配置不同,
有以下几个问题
1、是否能调整RAMP,COMP引脚参数做到兼容设计?
2、这个BUCK电路中,SW引脚对地是否需要加RC电路,参数如何选择?
3、如需外部开关控制这个电路,选择控制EN接地或者UVLO接地,哪个更合适?