This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5013: 我有一个LM5013的设计问题,按照datasheet中的推荐参数,在VIN=24V时,会出现双波的情况,而VIN=48V时,不会出现;

Part Number: LM5013

问题请教:

Question for advice:

按照datasheet中的参数设计,设计VOUT=12V,FSW=300K;在VIN=48V时,输出正常,而VIN=24V时,SW出现双波,频率也和设计不同;为什么会出现低压输入的这种双波?

According to the parameters in the datasheet, the design specifies VOUT = 12V and FSW = 300K. When VIN = 48V, the output is normal, but when VIN = 24V, a double wave appears at SW, and the frequency also differs from the design. Why does this double wave occur under low input voltage?

参数选取:

Parameter selection from datasheet:

VIN=24V,VOUT=12V,load=1.25A,SW及IL出现如下波形,频率变成了设计值的一半:

VIN=24V,VOUT=12V,load=1.25A,SW and IL exhibit the following waveform, the frequency becomes half of the designed value:

VIN=48V,VOUT=12V,load=1.25A,SW及IL出现如下波形:

VIN=48V,VOUT=12V,load=1.25A,SW and IL exhibit the following waveform: