Part Number: BQ24040
BQ24040DSQR 这个芯片在半成品测试时发现充电电流偏低,要求900mA±40mA,实际只有850mA左右。不良现象4%,以往正常的大部分都是890mA左右。批次是D/C2515.
请问为什么会这样呢?
第二个问题是这个充电电流公差应该是10%吗?是不是810mA-990mA都是正常的?但为啥这次的偏低呢,是否影响正常使用?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.