This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24040: 充电电流偏低

Part Number: BQ24040


BQ24040DSQR 这个芯片在半成品测试时发现充电电流偏低,要求900mA±40mA,实际只有850mA左右。不良现象4%,以往正常的大部分都是890mA左右。批次是D/C2515.

请问为什么会这样呢?  

第二个问题是这个充电电流公差应该是10%吗?是不是810mA-990mA都是正常的?但为啥这次的偏低呢,是否影响正常使用?

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 您好

    请提供更多背景信息。请提供示意图。当时的输入电压是多少,电池电压是多少?

    1. 输入电压5V
    2. 电池电压4.2V
    3. 引脚2 (ISET)接地电阻为634Ω±1%
    4. 根据规格书PIN2脚编程电阻来看设置900mA充电应该是594Ω才对,634Ω会不会偏大导致充电电流只有850mA,达不到900mA呢?
    5. 规格书里面2脚的电阻设置:Programs the Fast-charge current setting. External resistor from ISET to VSS defines fast charge current value. Range is 10.8k (50mA) to 540Ω (1000mA)
  • 您好

    对于50mA至1000mA的范围,KISET典型值为540AΩ。将KISET除以RISET(540AΩ/634Ω),充电电流为852mA。包含最大/最小值(不考虑电阻容差),最大/最小充电电流为899mA/804mA。要达到900mA的充电电流(ICHG),几乎不可能实现,因为这需要依赖电阻的容差来确保稳定达到900mA。如您所建议,请将ISET电阻更改为600Ω,以获得最大/最小值950mA/850mA。