Question 1: PPHV corresponds to a bidirectional 5A current; PP5V corresponds only to the switch used when acting as a source to output externally. When TPS25751D is used as a source, can it only use the switch corresponding to PP5V to output 5V externally? Is it still possible to use the PPHV path to output power externally?
Question 2: When TPS25751D is used as a sink, it can only use the built-in bidirectional PPHV 5A switch. Are there any requirements for the input voltage and current? Does it have to be above 5V?
Question 3: TPS25751D needs to detect DCIN12V and a tablet (which does not support PD) insertion, both detections being based on GPIO high/low level. Can the results of this detection be used to switch the internal switches corresponding to PPHV or PP5V? Can the corresponding software adjustments accomplish this?
Question 4: Below is a preliminary block diagram of one of our ideas. Are there any suitable I2C bidirectional buck-boost chips you would recommend? Requirements: Input: 12V / ≥5A; Output: 5V~20V / Current ≥3A.Question
5: Does the EEPROM need to be of a specific model? Could you help recommend one?