Part Number: TPS2663
Other Parts Discussed in Thread: BQ25690
Hello, we aim to implement a hardware circuit system architecture similar to the block diagram below.
Using a 24 V bus, with an input power supply of 24 V/1.5 A. This system incorporates a lithium battery pack and power path management (power multiplexing) circuitry to implement a cooperative power supply strategy: “light loads powered by the adapter alone, heavy loads powered by the adapter + lithium battery in parallel.” This ensures stable, continuous operation of the 24 V output under peak 5 A (or 7 A) conditions (with continuous output lasting approximately 10 minutes within an hour).
1. Light Load Mode (Iout ≤ 1.5 A):
The adapter directly supplies the load while simultaneously charging the lithium battery pack via a Buck charger. Input power takes priority, with charging current limited by input surplus.
2. Heavy Load Mode (Iout = 5 A/7 A):
Under input power current-limiting protection (protection threshold 1.5 A), the battery supplies power in parallel with the adapter via the power path/buck-boost conversion (load sharing) to jointly maintain the 24 V bus. The adapter outputs continuously up to its current limit, while the battery compensates for the current gap.

"Sorry! I had uploaded a block diagram elsewhere in the forum. Also, could you provide a detailed introduction on how to implement 'change dynamically by using DAC'?"