Other Parts Discussed in Thread: BQ24780S
Hi i have some problem with BQ24780S EVM Board, the VSYS output is abnormal, i have checked the BOM of the PCB Board, the VSYS droped after few pulse,the waveform shown as belows but i can normally accessed to the BQ Studio and can write&read register,i think it's weird,i also replaced 24780S and All Q1-Q5 MOS,still the same phenomenon,i cheked that the ACDET is 2.6V, ACOK 3.3V , REGN is 6V and Ilim>0.5mV, it's seemed that the ACDRV turn on is abnormal,could you give me some advice about that,does the board trigged the protection or the other schemetic components that i need to rechecked it, many thanks to your kindness help!
Red signal is Vsys blue is ACDRV and Green is CMSRC