This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478效率低下问题,求解答

Other Parts Discussed in Thread: LM3478, LM5175, LM25118, LM5122

制作一个产品前段是用LM3478做成的10-30VDC输入,19VDC-2A输出的一个DCDC转换,如图L4使用15uH 7A 20% CDRH1207,L5使用100uH 2.7A 20% CDRH1207,的电感,Q1使用AOD2908,D4使用50WQ10FNPBF,从负载100R一直到负载12R效率一直在81%附近,负载>1A,发热量L4>L5>Q1>D4(元器件上的温度),请帮忙分析一下,因为后面还要把振铃吸收掉,效率只可能更低了,都没法用了

RFFM-0107-V2.pdf