This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24251 充电电流500mA、2A的问题?

Other Parts Discussed in Thread: BQ24251

      RISET、RILIM已经通过外部的电阻进行配置了,充电电流最大为2A,输入电流最大也是2A。

      请问TI技术人员,现在如果不使用I2C对BQ24251进行配置(I2C_SCL,I2C_SDA已经断开),充电器已经对D+和D-短接了,BQ24251的D+和D-引脚接到外部的USB上,比如设备关机的时候,就是负载端没有负载,此时充电电流能达到1.3A左右。

      但是如果开机以后,就是负载端有负载了,此时插上USB充电,一会电流能到1.3A,一会只有500mA,非常不稳定,电池已经没有电了,可以确认。请问BQ24251的BC1.2检测sequence到底是个什么流程,另外TRM手册里面提到的power up,到底是USB插入时候呢,还是负载接入时?

  • 你好,换用一个输出能力更大的输入源看看是否因为功率路径管理的原因,导致芯片认为需要降低充电电流以优先满足负载需求。谢谢!

  • 我们用直流电源测试的,最大电流输出10A,电压5.1V(已考虑压降问题,所以调整为5.1V),直接将D+和D-短接,再进行测试:

    经过测试:

    1、如果SYS脚有400mA负载的话,充电电流最大只能到480mA,而且一直保持不变,如果负载端电流为5mA(系统进入休眠状态),此时充电电流能到1.4A左右,请问这是什么原因?

    2、如果D+和D-不短接,系统休眠,负载端为5mA,此时充电电流只有95mA,请问是什么原因?


    要求在USB不插入电脑时,充电电流能达到设定的最大值,如果USB插入电脑USB口,此时应该限流为500mA,请问应该如何改进?