Other Parts Discussed in Thread: BQ24251
RISET、RILIM已经通过外部的电阻进行配置了,充电电流最大为2A,输入电流最大也是2A。
请问TI技术人员,现在如果不使用I2C对BQ24251进行配置(I2C_SCL,I2C_SDA已经断开),充电器已经对D+和D-短接了,BQ24251的D+和D-引脚接到外部的USB上,比如设备关机的时候,就是负载端没有负载,此时充电电流能达到1.3A左右。
但是如果开机以后,就是负载端有负载了,此时插上USB充电,一会电流能到1.3A,一会只有500mA,非常不稳定,电池已经没有电了,可以确认。请问BQ24251的BC1.2检测sequence到底是个什么流程,另外TRM手册里面提到的power up,到底是USB插入时候呢,还是负载接入时?