This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL431使用发热讨论

Other Parts Discussed in Thread: TL431

各位:

在传感器项目中,考虑功耗较小,大概20mA的样子,于是乎使用了TL431将电压从30V稳压到5V,电路图如下,

1、初步测试,发现电压都正常,但是TL431管子发热比较严重(SOT23-3封装)

2、考虑到是否不稳定造成的震荡,示波器测试发现无震荡信号,但是一直比较热,搞不明白为啥

3、去掉图中的圈出的两个电容,老化测试,50多小时后发现,芯片TL431已经无法正常供电,输出只有2.5V左右,请有经验的人指导下,谢谢