各位:
在传感器项目中,考虑功耗较小,大概20mA的样子,于是乎使用了TL431将电压从30V稳压到5V,电路图如下,
1、初步测试,发现电压都正常,但是TL431管子发热比较严重(SOT23-3封装)
2、考虑到是否不稳定造成的震荡,示波器测试发现无震荡信号,但是一直比较热,搞不明白为啥
3、去掉图中的圈出的两个电容,老化测试,50多小时后发现,芯片TL431已经无法正常供电,输出只有2.5V左右,请有经验的人指导下,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位:
在传感器项目中,考虑功耗较小,大概20mA的样子,于是乎使用了TL431将电压从30V稳压到5V,电路图如下,
1、初步测试,发现电压都正常,但是TL431管子发热比较严重(SOT23-3封装)
2、考虑到是否不稳定造成的震荡,示波器测试发现无震荡信号,但是一直比较热,搞不明白为啥
3、去掉图中的圈出的两个电容,老化测试,50多小时后发现,芯片TL431已经无法正常供电,输出只有2.5V左右,请有经验的人指导下,谢谢
Hi
主要的电流来自Ika, 假设这个电流是2mA, 输出20mA, 那么电阻至少就需要小于(30-5)/(20+2)=1.13k.
所以本身你选择1k没有问题, 但是当输出假设只有2mA, 才是TL431就需要承受20mA, 5V输出功耗大约是0.1w.
即便热阻是259℃/W, 温升大约是26℃, 芯片的温度是51℃(常温下), 如果是高温换就你就要选择热阻尽量低的封装。
Hi
建议选择热阻比较低的封装。
电阻可以选择1k欧姆。