UCC28740: UCC28740:PMP41009

Part Number: UCC28740
Other Parts Discussed in Thread: PMP41009

Hello, I plan to use the UCC28740 chip to design a wide-range dual-transistor flyback converter with a structure similar to that of the PMP41009. Its specifications are as follows: output power of 40W, input voltage of 85-900V AC, output voltage of 24V, and maximum switching frequency of 100kHz. However, during the transformer design process, when calculating the primary inductance (Lp) in accordance with the UCC28740 datasheet, the resulting Lp value is 330μH. At this point, the minimum on-time (ton(min)) does not meet the minimum target of 280ns (maximum tCSLEB). Additionally, the calculated minimum required Lp value is 792.97μH. Does this mean that my design specifications are not achievable?Why is this the case, and which part of the designed specifications is unreasonable?

补充说明:

image.png

  • Hello, we have received your case and the investigation will take some time. Thank you for your patience.

  • 您好

    请选择最大工作频率为65至70KHz。

    试着遵循这个设计。我选择了你的CC功率为46瓦

  • Hello, thank you for your reply. However, I am required to use SiC MOSFETs in the design, so I hope the maximum frequency can reach 100 kHz to leverage the advantages of SiC. Could you please advise on the methods to achieve a maximum operating frequency of 100 kHz? In addition, the recommended design document in your previous reply failed to open; would you mind resending it? Thank you and best regards.

  • 您好

    Operating frequency max 100KHZ.

    With !0KHz I used 90KHz,

    Its just image. please use this values

  • Hello, why can't these two pictures you sent be displayed?

  • Hello, based on the parameters you provided, I calculated that the turns ratio between the primary winding and the auxiliary winding is 13. Is this parameter reasonable?

  • Hello, I have redesigned the transformer using the parameters you provided, but there has been no improvement at all — the duty cycle is still extremely small. In your opinion, what other aspects could be the cause of this problem?

  • 您好

    你能调节电压吗?你面临的实际问题是什么?

  • Hello, my problem is that the duty cycle of my MOSFET is incorrect. My design requires it to work properly within the 85-900VAC input range, but the current duty cycle is too small. Adjusting the voltage feedback section has no effect; only changing the current sampling resistor of the CS pin on the control chip and the relevant parameter values of the RC circuit can alter the duty cycle. However, after making these changes, the output voltage is too high under no-load conditions, and the duty cycle does not increase significantly either. So is there any solution to this problem? I am using a SiC MOSFET—does this have any impact?The first image shows the Vgs and Vds waveforms of the MOSFET with 220VAC input under no-load condition, and the second image displays the Vgs and Vds waveforms of the MOSFET with 220VAC input under half-load condition. The upper trace is Vds and the lower trace is Vgs.

  • My design is almost the same as that of PMP41009, with the only major difference being the addition of a driver chip in the driving circuit to drive the SiC MOSFETs. Could this be the cause of the problem? However, the waveform output by the control chip DRV is exactly the same as and perfectly matches the Vgs waveform of the MOSFETs. So I really have no idea where the problem lies right now. Could you help me figure it out? Thank you.

  • Dear expert,
    During debugging, I found that the operating frequency remains unchanged at only 16 KHz when the input voltage is set to AC 220V, 380V, 660V and 900V respectively. According to the design, the operating frequency of the converter should vary with different input voltages, with a maximum of 90 KHz. Could you please advise on what might be causing this issue?
  • Hi 

    Can you share me at what condition you are facing issue? Vin? vout? load? 

  • My question is why the operating frequency of my converter remains unchanged at different input voltages. Shouldn't the operating frequency of the UCC28740 chip vary accordingly? The test was conducted under heavy load conditions just now, and the output voltage only changed slightly, ranging from 23V to 24V.

  • Hello, I tested the prototype by varying the input voltage under heavy load conditions, with the input ranging from 220V to 900VAC. I found that the operating frequency of the converter remains constant at 16KHz, but the transformer you designed for me can achieve a maximum operating frequency of 90KHz. I believe the reason for this is that the chip has been operating in Constant Current (CC) mode. Could you please tell me how to switch it to Constant Voltage (CV) mode? I have replaced the resistance values of RFB3 and RFB4, which only increased the fixed frequency but still failed to switch it to CV mode.

  • Hello, I can now make my design output 24V under both heavy load and no-load conditions. However, the operating frequency remains fixed across different input voltages, which does not conform to the control method of the UCC28740. What steps should I take to make the control chip implement variable frequency control?

  • Another question is: For a dual-transistor cascaded flyback topology like the one designed in PMP41009, if the switching MOSFETs are replaced with SiC MOSFETs, is it necessary to add a gate resistor between the gate and source of Q2? And if added, will it have any impact on the operation of the circuit?