This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: VFB电压跳动

Part Number: BQ24610

VFB引脚电压跳变,VFB引脚测试出来时2.09V,但是有时候会瞬间变成2.01V,然后立马变回来,这就导致电池端口那里的电压跳动,导致在充电的时候会误判充电完成,然后要重新动一下板子,就有能立马充电了,这是什么问题,而且充电电流只有设定的一半,设置充电电流5A,那么实际充电电流就是2.5A,设置为3A,实际充电电流1.5A。