UCC28740: PMP41009

Part Number: UCC28740
Other Parts Discussed in Thread: PMP41009

Hello, I have designed an AC-DC flyback converter with an input of 85–900 VAC and an output of 24 VDC, adopting a two-switch cascaded flyback topology that is consistent with the design of UCC28740 chip and PMP41009. My questions are as follows:

  1. Is the design of the transformer in the picture correct?
  2. The duty cycle of my MOSFET is very small. I replaced the parameters of the relevant components in the voltage feedback loop, but there was no change. Only by increasing the parameter values of the RC circuit between the control chip CS pin and the sampling resistor in the current sampling circuit can the duty cycle be increased, and changing other parameters has no effect. The output voltage of the flyback converter is normal under no-load and light-load conditions, with the duty cycle remaining at a very low level (appearing as a flat line). However, under heavy-load conditions, the duty cycle is still very small and the output voltage drops to around 15V. What could be the possible reasons for this phenomenon?a2890dc90a3d393213f5de076df3eb6a.jpg
  • As mentioned, Pout = 46.31W and Vout = 24V is desired at full load condition, that means Iout = 1.9298A.

    And I_load_CC is mentioned as 1.875A, so under full load condition converter will enter into CC mode.

    So i would suggest to increase CC limit and that will be done using CS pin resistors only, and so you find that changing CS pin resistor, duty cycle is increased since CC limit is changed. 

  • So, what should I do now? Should I increase the resistance of the CS pin? What about the capacitance value? Should I increase both of them? However, increasing the RC values will result in loud transformer humming. Could you please give me some advice?

  • I'm not operating at full load — only at half load.

  • Decrease value of Rcs to have CV mode upto full load. Capacitance at CS pin is just for filter. Refer to 10.1.5 of datasheet---(A small filter capacitor may be placed on CS to GND, with short traces, to filter any ringing that may be present at light load conditions when driving MOSFETs with large gate capacitance. This capacitor may not be required in all designs.)

  • The value of RCS has dropped to 0.35 ohms. Do we need to lower it further?

  • Use value of Rcs as per equation 14 given in datasheet.

  • Hello, I haven’t been able to find the waveform diagram of the MOSFET Vgs for the flyback converter designed with the UCC28740 chip. It seems that only the Vds waveform diagram is available. Could you please help me find the Vgs waveform diagram?

  • yes, test report doesn't have VGS waveform and i don't have PCB to test and provide you. What is issue you are facing ?

  • Hello, my problem is that the duty cycle of my MOSFET is incorrect. My design requires it to work properly within the 85-900VAC input range, but the current duty cycle is too small. Adjusting the voltage feedback section has no effect; only changing the current sampling resistor of the CS pin on the control chip and the relevant parameter values of the RC circuit can alter the duty cycle. However, after making these changes, the output voltage is too high under no-load conditions, and the duty cycle does not increase significantly either. So is there any solution to this problem? I am using a SiC MOSFET—does this have any impact?The first image shows the Vgs and Vds waveforms of the MOSFET with 220VAC input under no-load condition, and the second image displays the Vgs and Vds waveforms of the MOSFET with 220VAC input under half-load condition. The upper trace is Vds and the lower trace is Vgs.

  • My design is almost the same as that of PMP41009, with the only major difference being the addition of a driver chip in the driving circuit to drive the SiC MOSFETs. Could this be the cause of the problem? However, the waveform output by the control chip DRV is exactly the same as and perfectly matches the Vgs waveform of the MOSFETs. So I really have no idea where the problem lies right now. Could you help me figure it out? Thank you.

  • what is value of RCS connected in PCB now?

    what is o/p voltage at no load and half load condition with 220V AC?

    can you provide CS and VS pin waveform for no load condition with 220VAC ?

  • Currently, the resistance value of RCS is 0.55Ω. The output voltage is 24.1V under no-load condition and 14.4V under half-load condition. The first figure shows the VS pin voltage waveform under no-load condition, and the second figure shows the CS pin voltage waveform under no-load condition.

  • At no load condition, o/p is 24V as designed. So i think at no load condition, there should be no issue. Since you mentioned previously that at no load condition, o/p is too high. but it is within desired value.

    Can you provide CS pin waveform aligned with VDS and clearly showing magnitude at turn on period and at turn off period ?

  • Hello, due to the limitations of experimental conditions, I am unable to provide the waveforms of Vds and CS simultaneously and have to present them separately. Figure 1 shows the Vds and Vgs waveforms of the MOSFET under half-load conditions, and Figure 2 displays the voltage waveform of the CS pin under the same half-load conditions. Could you please give me some suggestions on what modifications I should make next?
  • Hello, the turn ratio of my transformer is set to Np:Ns:Na = 42:6:4, and I’ve selected RVS1 as 42.2 kΩ and RVS2 as 13 kΩ. Do these two parameter values need to be adjusted?

  • What is value of cap on CS pin? And Vout is not regulated to 24V, right?

  • Yes, the output voltage is only 17V at half load, and the capacitor at the CS pin is 1nF.

  • Dear expert,
    During debugging, I found that the operating frequency remains unchanged at only 16 KHz when the input voltage is set to AC 220V, 380V, 660V and 900V respectively. According to the design, the operating frequency of the converter should vary with different input voltages, with a maximum of 90 KHz. Could you please advise on what might be causing this issue?
  • If switching frequency is not changing that means VCL (internally generated) is not changing which is based on IFB current. Check IFB pin waveform.

  • You're right, but how should this problem be solved? I have swapped out all the components related to the voltage feedback loop connected to the FB pin, yet it still doesn't work. Why is that?

  • Hello, I tested the prototype by changing the input voltage under heavy load conditions, with the input ranging from 220V to 900VAC. I found that the operating frequency of the converter remains constant at 16KHz, but the maximum operating frequency I designed is 90KHz. I think the reason for this phenomenon is that the chip has been working in Constant Current (CC) mode. Could you please tell me what I should do to switch it to Constant Voltage (CV) mode?