目前TI官网看到LM5085外围比较简单,但是效率稍低,75-78%左右,由于不是同步整流,不知道二极管和MOS在5-6A发热是否会很大。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
满载效率有点偏低,注意一下选择的器件,如电感(低DCR),肖特基(低Vf)等。
您可以用TI的wenench仿真得到电路的相关参数,例如5~6A,效率在81~82%左右。
这个软件可以用于器件选型,包括芯片以及外围器件。
Hi
补充:
仿真得到肖特基的温度大于在131摄氏度(Vf=4.55V,Io=6A)