如题,TI员工能否推荐个:低输入/输出电容的DCDC,电感最好较小,输入9~24V,输出3A,效率当然越高越好啦。
前代产品用的LM2675,由于新产品的电流增加了约10倍,上次测试用2675带不起来了,在ti官网用那个设计器没有找出一个器件来
我这里有没有北京这边的TI技术支持电话,古来次发帖求助
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
可以参考LM43603,效率较高且开关频率可调,所以这样你可以设置较高的开关频率来减小电感体积。
但是需要注意,效率和开关频率是一个折中,所以建议你选取不要高于800kHz的开关频率,否则热也会比较难设计。
关于设计可以用Webench设计工具,TI.COM右下角。
你好
1. 确实,2M开关频率发热会很严重,也就是说你的输出电流需要降额使用,或者地必须铺得很好,另外一个就是开关频率2M对布板的要求确实也较苛刻,当然你可以尝试;
2. LM2596这些确实是LM比较老的芯片,开关频率一般只有150KHZ,所以相应输出电感和电容会比较大,所以你可以尝试LM43603,这样设计会更符合你的要求。