Other Parts Discussed in Thread: BQSTUDIO
在官方BQ34Z100PWR-G1 电池计量芯片数据手册内,表7-1 Data Flash Summary(Continued)内,Design Energy Scale 这一变量最大值为255,最小值为0,但是在7.3.6.5 Design Energy Scale 内描述为“Design Energy Scale is used to select the scale/unit of a set of data flash parameters. The value of Design Energy Scale can be between 1 and 10 only.
When using Design Energy Scale > 1, the value for each of the parameters in 表 7-15 must be adjusted to reflect the new units.”,这里要求Design Energy Scale 这一变量的范围为0-10;
Design Energy Scale这一变量的具体值范围是多少?这一变量的具体含义是什么?是不是需要搭配Design Energy 这一变量配置?