This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350R1 shutdown关机后,重新开机容量不准问题

Other Parts Discussed in Thread: BQ76930

BQ78350R1+BQ76930方案

充电充满后,100%  从上位机battery manage发送shutdown关机命令,然后按键开机,容量就变为65%

试过无数次都是这样,然后再用小电流冲冲又会变回100%,但是开始放电的话,就会从65%开始降低

这是为啥?BUG?

我们的电池还未校准 max error 2%左右,不知道跟这个有没关?如果有关,怎么快速的去校准max error 在理想的值,TI的代理也说得不明不白的,也没什么详细的资料,

  • BQ78350R1是采用CEDV算法,CEDV算法要获得准确的SOC,是需要经过一个满充满放的循环的。发送了Shutdown命令再唤醒,CEDV算法对初始容量的估算会有一定的误差。至于这么大的误差,可能你用的是磷酸铁锂电芯。



  • 至于有误差也不可能这么大,我们用的是三星18650电池。充放电一致性都比较理想的。在官方开发板测试都是一样的问题

    比如关机前和关机再开机电池电压都是没有变化的,但是容量就突变降低很多,这应该是个BUG,你们能重视去测试一下我这个现象吗?