This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS923652: TPS923652: TPS923652 may be damaged during use

Part Number: TPS923652

It is designed to drive a 24V 0.4A high-brightness screen.
The frequency is set at 400KHZ, and the MCU is used to send a 10KHZ PWM signal to the ADIM PIN as analog dimming.
During the testing process, TPS923652 was occasionally damaged.
We designed it in mid-2024. In the latest data manual, we found that CSN and CSP have a set of RC.
Datasheet says it is optional and is for noise filtering purpose.
However, we didn't reserve a position for R, so we came up with an alternative solution. We pulled down a set of R+C to ground at the SW end. The resistance of R is 10 ohms, and the capacitance of C is 4.7nF. So far, no damage has occurred during testing. Could this also solve the damage issue?Or is there any risk associated with this RC?