Part Number: BQ25730
在查阅BQ25730芯片手册中,发现“最大输入电流限制配置表”没有标注在采用4.7uH电感器下的最大输入电流配置信息,但EVM使用了4.7uH电感器。请问在采用4.7uH电感且开关频率在400K的情况下能否实现10A的最大输入电流,如果可以,EN_FAST_5MOHM与RSR_RAC BIT应该如何配置?文档中相关说明如下所示:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ25730
在查阅BQ25730芯片手册中,发现“最大输入电流限制配置表”没有标注在采用4.7uH电感器下的最大输入电流配置信息,但EVM使用了4.7uH电感器。请问在采用4.7uH电感且开关频率在400K的情况下能否实现10A的最大输入电流,如果可以,EN_FAST_5MOHM与RSR_RAC BIT应该如何配置?文档中相关说明如下所示:

您好
8.3.5 Input and Charge Current Sensing
8.6.23 IIN_HOST Register (I 2C address = 0F/0Eh) [reset = 2000h]
datasheet这两个部分由详细说明,如说明中相关配置请根据实际情况选择,且每个范围均有波动,您可以根据您实际情况来参考