Part Number: LM5148
我在使用TI提供LM5148的demo板上测试了一下负载调整率大概会有12%;给demo板的输入电压是19V,输出12V,负载从空载到10A的跳变过程发现输出电压会突变到13.5V,而手册上负载调整率只标了0.1%。贵司有没有相关负载调整率的实测数据和波形呢?负载波形如下图所示;
我自己的板卡是19V输入,输出5V,同时这个5V会给到VCCX引脚;在某一次测试中,多次上下电测试,发现VCCX引脚内部对地短路了,这颗芯片的VCCX引脚手册里写的是6.5V电压范围,在论坛中有看到有个FAE说VCCX引脚只能在5.5V以内;请问这个引脚在芯片内部有什么保护吗?