Part Number: UCC25661



Part Number: UCC25661



Thanks for your reply.I would like to add some additional information.I am not using PFC; the circuit is directly powered by an AC supply.The primary turns of the LLC transformer are 15, while both the auxiliary winding and secondary winding have 3 turns each.The chip I am using is the UCC256610.The parameters for the BLK pin, LL pin, and TEST pin are shown in the figure.I would like to clarify that the brown‑in voltage of the LLC is different from the value in the Excel sheet. According to my resistor values, the actual brown‑in voltage of the LLC is 355 V.Moreover, I am unable to plot the curve between Pin and VFB on my own.What I want to express is that the Pin‑versus‑VFB curve in the Excel file is for reference only.The resistor settings for both the LL pin and TEST pin are identical to those in the Excel spreadsheet.

In addition, the RISNS resistor I used is not 150Ω but 75Ω. Since the soft start of the UCC256612 cannot be configured, OCP is easily triggered during soft start when a 150Ω resistor is employed.
Thank you for your reply. The screenshot below shows the key parameters in the schematic I am using, along with the corresponding design calculation results.
Item A32 in the calculation table should be 420 V, but I am unable to edit this value in the table. The primary turns of the transformer are 15 and the secondary turns are 3, resulting in a turns ratio of 5, which also cannot be modified in the calculation sheet.Additionally, please disregard cells A254 and A279 in the calculation table. I have not altered these two parameters, as they are irrelevant to the issue I am encountering.
After further consideration, I suspect the problem may be related to the following factor:Since the unit is directly powered by an AC mains supply, the ripple on the DC bus voltage is relatively large, which leads to the coexistence of HF switching and normal switching.This is because the circuit board is not equipped with a PFC stage.
Yesterday, I used a 420 V DC power supply to directly feed the DC bus. The captured waveform at full load is attached below, though I am unsure if there is any correlation between the two test conditions; the above is only my preliminary speculation.I currently lean toward loop response issues as the root cause. Unfortunately, I have iteratively adjusted the loop parameters multiple times, yet the problem cannot be effectively resolved.
Thank you for your careful review and support as a TI application engineer.




如果只将RBLK下限值改为90K,那意味着LLC的brown in电压会很低。即便曲线可以变陡, 但应用不到实际吧。我修改了TEST引脚部分的电阻,将曲线往上移动,不会再出现两种模式共存的问题。但是我在全功率段调整负载时,发现即便是空载,电源也无法进入LF Burst,这是否意味着,对于曲线而言,最低点太高,而LF Burst的LF Burst Entry点还是小于曲线的最低点,因此电源无法进入LF Burst Entry。



这种设置下,我的电源不会再存在两种工作模式并存的现象。但正如我之前提到的,电源无法进入LFBurst,是否和LF Burst Entry这个电压太高有关?
另外,我的电源是240W的,我的曲线在满载的时候,FB只有2.3V,其实这个值是偏小的对吧,意味着OPP的时候功率会很大。
你好,
您的系统是否仅在轻负载下以高频脉冲串模式运行?
请分享设计计算器中的LL引脚设置部分。
此外,我的电源是 240W 的,我的曲线显示满载时 FB 电压只有 2.3V。这个值实际上偏低,这意味着启用 OPP 模式后功耗会非常高。
你的OPP极限值与你的功率水平相差甚远。
你需要选择合适的BLK引脚电阻,使得在标称输入电压下,BLK引脚上的等效电压约为4V。(因为UCC256610和UCC256614的扩展增益范围功能已启用)。否则,你的Vfbreplica与引脚关系图将呈直线,并且你会看到控制器在正常模式和突发模式之间来回摆动。
正如我之前提到的,由于所选部件具有 EGR 功能,因此您还需要更换 BLK 电阻器。
请发送更新后的设计计算器。
问候,
亚米尼。
"你的系统是否仅在轻负载下以HF Burst模式运行":是的。如果负载更轻,我希望系统会从HF Burst切换到LF Burst。但目前即便是空载,系统也不会进入LF Burst。

你好,这是我的LL设置部分。我很想知道为什么要把VLLB/LF Burst设置成固定的0.6?这意味着VLLB/HF Burst的值必须要小于0.6,表格里仅有0.55 0.5 0.45这三种选项。
对于BLK电阻的选择,我目前使用的upper电阻是11.75M,lower电阻是36K。实在抱歉,我想了很久,也没有明白你说的“使得在标称输入电压下,BLK引脚上的等效电压约为4V。(因为EGR功能)”确定4V没有打错吗?
你好,
在相同的输入电压下,启用 EGR 的版本比未启用 EGR 的版本增益更高,因为 BLK 会与 TSET 和 ISNS 一起影响增益。
通常,我们选择 BLK 电阻时,会确保标称输入电压下的 VBLK 约为 1.5V。但对于 UCC256610 和 UCC256614,我们选择 BLK 电阻时,会确保 BVLK 约为 4V。
你需要提高突发阈值才能进入低频突发模式。
您分享了LO的波形。
VLLB/LF 内部已固定,以便于选择 LL 引脚电阻。是的,您需要在 0.5、0.55 和 0.45 之间选择一个电阻值,才能同时获得高频和低频脉冲。
问候,
亚米尼。
Sorry for the late reply. I just got back from the Labor Day holiday, wish you happiness every day.
Given the EGR function of the UCC256610, does this mean it can support a lower input voltage?
Really sorry. I still don’t quite understand why the voltage on the BLK pin you mentioned is around 4V. I’ve taken a screenshot of my calculation process for the BLK resistor. Could you please help check where I made a mistake and where exactly this 4V comes into play?
For the UCC256610,VBLK_stop=1V ,VBLKstart_hys=0.05V,IBLK_sink=1uA;
RBLK_upper=11.8M,RBLK_lower=36K 。According to the datasheet, the calculation process is as follows.

Do you mean the voltage of VBLK_start should be 4V?
Thank you so much for your help these days. Thanks again!
What you mean should be: When the PFC is operating normally, the VBLK voltage should be 4V instead of 1.5V. That’s why you previously suggested changing RBLKupper to 90kΩ. The calculations for RBLKupper at 36kΩ and 90kΩ are as follows. However, there is an issue when RBLK is set to 90kΩ: the Vbrown_in voltage will become very low. Will this cause any problem when applied in the LLC topology? The loop gain will be extremely high under this condition.


你好,
在相同的输入电压下,启用 EGR 的版本比未启用 EGR 的版本增益更高,因为 BLK 会与 TSET 和 ISNS 一起影响增益。
通常,我们选择 BLK 电阻时,对于标称输入电压,VBLK 应约为 1.5V。但对于 UCC256610 和 UCC256614,我们选择 BLK 电阻时,BVLK 应约为 4V。
[/引用]在这种情况下,根据您的计算,Vbrown_in 为 150V 是正确的,因为 UCC256610 预计在宽输入范围内工作,因此 brown_in 电压预计也会很低。
如果您使用 PFC 并且 BLK 电压已调节,则可以使用 UCC256611,其中 EGR 已禁用,您可以将 1.5V 作为 BLK 引脚的标称电压,并获得更高的 brown_in 电压,但您必须重新设计控制器外围设备。
问候,
普里坦
你好,
在相同的输入电压下,启用 EGR 的版本比未启用 EGR 的版本增益更高,因为 BLK 会与 TSET 和 ISNS 一起影响增益。
通常,我们选择 BLK 电阻时,对于标称输入电压,VBLK 应约为 1.5V。但对于 UCC256610 和 UCC256614,我们选择 BLK 电阻时,BVLK 应约为 4V。
[/引用]在这种情况下,根据您的计算,Vbrown_in 为 150V 是正确的,因为 UCC256610 预计在宽输入范围内工作,因此 brown_in 电压预计也会很低。
如果您使用 PFC 并且 BLK 电压已调节,则可以使用 UCC256611,其中 EGR 已禁用,您可以将 1.5V 作为 BLK 引脚的标称电压,并获得更高的 brown_in 电压,但您必须重新设计控制器外围设备。
问候,
普里坦
你好,
在相同的输入电压下,启用 EGR 的版本比未启用 EGR 的版本增益更高,因为 BLK 会与 TSET 和 ISNS 一起影响增益。
通常,我们选择 BLK 电阻时,对于标称输入电压,VBLK 应约为 1.5V。但对于 UCC256610 和 UCC256614,我们选择 BLK 电阻时,BVLK 应约为 4V。
[/引用]在这种情况下,根据您的计算,Vbrown_in 为 150V 是正确的,因为 UCC256610 预计在宽输入范围内工作,因此 brown_in 电压预计也会很低。
如果您使用 PFC 并且 BLK 电压已调节,则可以使用 UCC256611,其中 EGR 已禁用,您可以将 1.5V 作为 BLK 引脚的标称电压,并获得更高的 brown_in 电压,但您必须重新设计控制器外围设备。
问候,
普里坦
很感谢你的回复,你的回复对我很重要。那也就是说,当我决定使用UCC256610,并且前级没有PFC,就是一个宽范围输入。在我设计LLC变压器参数的时候,我必须考虑到brown in电压很低的问题,也就是说哪怕brown in电压很低,只有150Vdc,我的LLC的增益曲线也必须满足。因为现在我的前级是有PFC的,如果按照你的建议,改变BLK下分压电阻,电源的brown in电压变得很低,我是不是得重新设计变压器参数。
很感谢你的回复,你的回复对我很重要。那也就是说,当我决定使用UCC256610,并且前级没有PFC,就是一个宽范围输入。在我设计LLC变压器参数的时候,我必须考虑到brown in电压很低的问题,也就是说哪怕brown in电压很低,只有150Vdc,我的LLC的增益曲线也必须满足。因为现在我的前级是有PFC的,如果按照你的建议,改变BLK下分压电阻,电源的brown in电压变得很低,我是不是得重新设计变压器参数。