This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76003: 关于LM76003的设计问题咨询

Part Number: LM76003

1、BIAS引脚在输出24V条件下,是不是应该悬空?

虽然手册中介绍了BIAS的最大值可以到30V,但是在LM76003: BIAS 腳位功能 - 电源管理论坛 - 电源管理 - E2E™ 设计支持 这个帖子中建议BIAS电压小于18V

2、在SW引脚是否可以增加串联的RC到地,改善SW开关波形

3、FB引脚输入是否可以增加一个RC滤波,使得反馈给FB引脚的电压更稳定

4、如果采用外部DAC调压,电阻R1/R2/Rdac的连接是不是如图上所示,以及调压Vdac和输出Vout的计算式为:[(Vout-VFB)/R1]+[(Vdac-VFB)/Rdac]=VFB/R2