This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS43060: TPS43060无法正常工作

Part Number: TPS43060

hello,我在使用TPS43060的过程中,将24V升压至26V,出现了两个问题,

  1. 上电瞬间,pin12,也就是SW脚损坏,共计7片,损坏了6片了,其中大约有4片是能看到火花的出现;
    在更换我从另外一家购买的TPS43060之后,不再损坏IC,两款芯片的尾缀不同。
    电路原理图如下:
    image.png
  2. 在更换IC之后,发现芯片温度很大,使用热成像观察有80度以上,请问这个问题如何解决?
    3169fdc02d63c3133574c07bb9bb45b4.jpgimage.png