This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409HV: LM3409HV在72V输入条件下,最大输出电流可以多少?PMOS管有型号推荐吗?

Part Number: LM3409HV
Other Parts Discussed in Thread: LM3409

LM3409HV在72V输入条件下,最大输出负载电流可以多少A?PMOS管有型号推荐吗?

  • 您好

    When designing, the maximum attainable LED current is not internally limited because the LM3409/09HV is a controller. Instead it is a function of the system operating point, component choices, and switching frequency allowing the LM3409/09HV to easily provide constant currents up to 5A. This simple controller contains all the features necessary to implement a high-efficiency versatile LED driver.

    PMOS管有型号推荐吗?

    没有相关针对性推荐。