Part Number: LM3409HV
Other Parts Discussed in Thread: LM3409
LM3409HV在72V输入条件下,最大输出负载电流可以多少A?PMOS管有型号推荐吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
When designing, the maximum attainable LED current is not internally limited because the LM3409/09HV is a controller. Instead it is a function of the system operating point, component choices, and switching frequency allowing the LM3409/09HV to easily provide constant currents up to 5A. This simple controller contains all the features necessary to implement a high-efficiency versatile LED driver.
PMOS管有型号推荐吗?
没有相关针对性推荐。