This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1 AFE 的过流跟短路保护 真的 不能自己恢复吗



前几天发表过一次 关于AFE 保护后 能不能自动恢复,但是有人知恢复说 只能reset,AFE保护后不能自动恢复。但是 我在想,终端客户拿到了电池,不小心短路保护了,想恢复 不是很麻烦。而且数据手册 里面明明写了恢复时间,为什么我新做的电池 在ASCC后不能恢复。

  • 请参考技术参考文档里的相关描述,如下:

    In general, when a fault is detected after the Delay time, both CHG and DSG FETs will be disabled (Trip
    stage), and an internal fault counter will be incremented (Alert stage). Since both FETs are off, the current
    will drop to 0 mA. After Recovery time, the CHG and DSG FETs will be turned on again (Recovery stage).


    If the alert is caused by a current spike, the fault count will be decremented after Counter Dec Delay
    time. If this is a persistent faulty condition, the device will enter the Trip stage after Delay time, and repeat
    the Trip/Latch Alert/Recovery cycle. The internal fault counter is incremented every time the device goes
    through the Trip/Latch Alert/Recovery cycle. Once the internal fault counter hits the Latch Limit, the
    protection enters a Latch stage and the fault will only be cleared through the Latch Reset condition.

  • 英文 看的有些蒙,你能不能大概帮我 描述一下 表达的意思。

  • 我把AOLatch Limit 次数由0设置为100次,每次的短路后立马断开,这样就可以自动恢复。如果不断开,通讯也会断开,激活MOS后 通讯跟MOS都恢复正常。 

    也就是说,报警的次数越过了设置的次数,就会进入锁住保护的阶段 latch stage。而出厂状态下为0次,所以一旦发生trip/latch/ alert 保护后,立马锁住,只能通过reset 恢复。

  • 恢复的条件就是“Latch Reset condition”,不同的dataflash配置,如NR bit,恢复的条件不一样。

  • 恩,我PRES pin没有使用,现在设置成NON-REMOVABLE mode后,恢复就是 靠延时了。 怪不得 我之前感觉短路了,恢复时间那么短,根本没有默认的5S那么长。