This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: programmable DC power supply

Part Number: TMS320F280049C

Dear TI Technical Experts,
I plan to develop a programmable DC power supply with the following key specifications:
  • Output voltage: 0~20 V DC
  • Output current: 0~200 A
  • Rated output power: 4000 W
  • Input power: compatible with single-phase AC 220 V or three-phase AC 380 V
  • Control modes: Constant Voltage (CV) / Constant Current (CC) / Constant Power (CP)
  • Industrial communication & analog interfaces: RS485 Modbus, 4–20 mA analog signal and 0–10 V analog signal
Could you please recommend applicable design solutions?