Part Number: BQ25896
我们现在测试VBUS输入电压低于4.5V时(未接电池),25896寄存器显示no adapter,VSYS也不正常,输入电压最小值不是3.9V吗?这个现象正常吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ25896
我们现在测试VBUS输入电压低于4.5V时(未接电池),25896寄存器显示no adapter,VSYS也不正常,输入电压最小值不是3.9V吗?这个现象正常吗?
您按照手册16,17,18页的 Device Power Up from Input Source逐步检查一下
我们试了4.1V,4.2V,4.3V,4.4V,电流可达3A,与手册对比,这个电源条件是满足手册要求的,但寄存器显示no adapter,VSYS也是一个跳动的数值