This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS26742EQ1EVM: TPS26742 規格詢問

Part Number: TPS26742EQ1EVM

Dear Sir,

請問TPS26742 是否可以支持下列規格, 如果不行是否有其他建議的使用料?

Input +24VDC +-10%

Output 1: Legacy USB-A Fast-Charging Port

Support: BC1.2, QuickCharge4.0, Legacy Apple resistor schemes

 

Output2: 100W USB-C Fast-Charging Port

Support: PD3.1, QC4/4+

 

Best Regards,

Grace