请问各位专家,这个芯片的OTG,和咱们通常意义的on the go 有什么关联吗?
通常意义的:OTG技术就是实现在没有Host的情况下,实现设备间的数据传送。
我仔细看了datasheet,看不出咱们芯片上的OTG PIN 跟上面这个概念之间有任何联系,求解释!
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ24195的电源部分实际上等效于一个双向电源,充电时buck,做OTG时boost。
因为单节电芯只有4.2V,所以如果要OTG给其他设备通过USB供电,那么需要将4.2V升压为5V作为USB母线电压,即反向时的boost工作状态。
以上谢谢!