Part Number: BQ25619
BQ25619芯片的QON引脚空载时电平只有2.6-2.7V,QON引脚外接按键,BQ25619芯片进入运输模式后,短按按键2秒,芯片不能退出运输模式,V_SYS电压1.4V,接USB能退出运输模式,请问QON电压正常吗,为什么不能退出运输模式?
已经收到了您的案例,调查需要些时间,感谢您的耐心等待。
关于BQ25619退出运输模式,,请参考数据表的7.3.7.2 BATFET Enable (Exit Ship Mode):
“A logic high to low transition on QON pin with tSHIPMODE deglitch time to enable BATFET to exit ship mode.”
tSHIPMODE的时间是 0.9s ~ 1.3s
QON引脚的内部上拉电平是多少?,QON引脚空载时电平是多少?
The pin is pulled up to VBAT through 200 kΩ to maintain default HIGH logic during Ship mode. It has an internal clamp to 6.5 V.
请问你们有实测过QON的电平吗,具体数值是多少?
请问这个是对的吗
能给我发下链接吗?
[参考译文] BQ25618E:/QON 电压 - 电源管理(参考译文帖)(Read Only) - 电源管理(参考译文帖) - E2E 设计支持
可以参考,下面是原链接:
BQ25618E: /QON voltage - Power management forum - Power management - TI E2E support forums