This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79600-Q1: BQ79600-Q1通信时间相关问题

Part Number: BQ79600-Q1
Other Parts Discussed in Thread: BQ79758B-Q1, BQ79616-Q1

您好,我们现在使用BQ79600-Q1 作为base device,BQ79758B-Q1和BQ79712B-Q1作为stack device,BQ系列设备之间通过SPI和菊花链进行通信  ,我想知道主机发送命令需要等待后多久后可以再发送下一条命令

现在我们会使用下面三种命令,请确认下我的等待的时间是否正确

①写入 

等待时间= SPI通信时间+Total wait time 250μs

 

②读取 base device 的数据

等待时间=SPI通信时间 +  tWAIT_READ_MAX

 tWAIT_READ_MAX =100μs + m*10μs 

 

③读取  stack device 的数据

等待时间=SPI通信时间 +  tWAIT_READ_MAX

 tWAIT_READ_MAX = (n-1)*3μs*2 + m*10μs + 100μs. 

 

之前的提问中我了解到3μs不是固定值,而是3us是stack设备reclock的时间,以stack芯片数据手册为准。 

但对于10μs还有疑问,回答为Byte delay (including reclocking time)的时间,B0 starts forward after the 1st byte is received.  但对应BQ79616-Q1 Daisy Chain Communications  中12μs,和公式中不同,请问具体怎么得到该时间,实际应该参考什么资料才能确保等待了足够的时间